Fast Fourier transform

Brief Description

File: \examples\Processing\FastFourierTransform\mE5-MA-VCL\fft.va

File: \examples\Processing\FastFourierTransform\iF-CXP12-Q\fft.va

Default Platform: mE5-MA-VCL and iF-CXP12-Q

Short Description

Shows the usage of operator FFT. The applet generates a sine pattern and performs the FFT. The results show the frequency part. Use the VisualApplets simulation.

The provided example will demonstrate the use of the FFT. In the example, a simple sine wave with period 256 and magnitude ± 16384 and an image width of 2048 pixels is generated.

Sinewave

Figure 296. Sinewave


The VisualApplets implementation is very simple. A sine wave input is forwarded to the FFT operator. The resulting real and imaginary part are squared and added. So the output is the squared absolute value. The result shows the expected peak at x = 8 i.e. a period of 2048 / 8 = 256. A comparison with Matlab FFT calculation shows a very similar result in the same accuracy range. H-Box "DynamicReduceResolutionFFTOut" is used to shift results and reduce their resolution. This is not required for the given sine wave but is an option for other requirements.